AXIS#.EIP.STREAMPERIOD
Description
This parameter allows modifying and configuring the interval at which the drive expects to receive position set-points from the fieldbus master when position streaming is configured and enabled (AXIS#.EIP.STREAMING = 1).
Example
-->AXIS1.EIP.STREAMPERIOD 500 -->AXIS1.EIP.STREAMPERIOD 500 [us]
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-11-00-001 |
General Information
|
Type |
Read/Write |
|
Units |
Microseconds |
|
Range |
500 to 10000 |
|
Default Value |
2000 |
|
Data Type |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
7537 |
1 |
7537 (0x1d71) |
AXIS1.EIP.STREAMPERIOD |
Signed32 |
Read/Write |
Yes |
|
73073 |
2 |
7537 (0x1d71) |
AXIS2.EIP.STREAMPERIOD |
Signed32 |
Read/Write |
Yes |